This object contains attributes common to many Metasys system objects. These common attributes are described in the Common Object Attributes section.
|
Attribute Name |
Notes |
Description | ||||||||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
Display Reference |
N |
Represents the label of the Display Attribute. The Display Reference is not stored in the object, but read when requested. |
||||||||||||||||||
|
Target Reference |
Identifies the source that provides the data elements linked to the individual attributes of the GIO. | |||||||||||||||||||
|
Attribute Info |
C,W |
Contains a list of structures that store data about each
attribute defined within a GIO. The elements listed in this
table appear as columns on the Hardware tab of the Configure
screen of the Insert Point Wizard - GIO.
|
||||||||||||||||||
|
Display Attribute |
C |
Specifies the attribute that represents the value of the GIO. The value of this attribute is used as the Present Value of the GIO. For example, for a GIO representing a temperature control strategy, you might choose the attribute representing room temperature to be the Display attribute. Then, the room temperature appears as the GIO Present Value. |
||||||||||||||||||
|
Remote Object Name |
C,W |
Contains the name of the object in the format of system.object. | ||||||||||||||||||
| GIO 1 Attr. . .GIO 256 Attr |
W |
Represents user-definable attributes that can be part of a GIO. Each attribute represents a potential entry in the Attribute Info attribute which in turn represents a physical or logical piece of data within an integrated device. These attributes only appear on the Hardware tab of the Configure screen of the Insert Point Wizard - GIO. |