BACnet IP Integration Object Commands - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The following table lists the commands supported by the BACnet IP Integration Object.

Table 1. BACnet IP Integration Object Commands

Command Name

Parameters

Description

Sync Field Device Times

None

Sends a high-priority time synchronization command to all child BACnet IP Integration devices, based on each device mapper object's Manual Time Sync Type attribute.

If the Manual Time Sync Type is set to:

  • UTC: UTC time synchronization message is sent.

  • Local: a local time synchronization message is sent.

  • None: no message is sent.

  • Auto: the mapper object's Protocol Services Supported attribute is used to determine which type of time sync is supported, and if:

    • utcTimeSynchronization is set, the code functions as if Time Sync Type is set to UTC.

    • utcTimeSynchronization is not set and timeSynchronization is set, local time is sent.

    • neither utcTimeSynchronization nor timeSynchronization is set, no time is sent.