BACnet IP Integration Object - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The BACnet IP Integration object manages the communication with a BACnet/IP network. All integrated BACnet devices and objects appear under the BACnet IP Integration object in the Navigation Tree.

The BACnet IP Integration object serves as the root for all integrated BACnet/IP Field Controller objects on an Ethernet trunk. The BACnet IP Integration object is a direct child of a supervisory controller and integrates BACnet/IP devices using the Ethernet trunk.

For general information on Metasys system objects, see the Object Help section.

For detailed information on the BACnet IP Integration object, see BACnet IP Integration Attributes.