Monitoring and Commanding Items Using Graphics in View Mode - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

About this task

Note: The Metasys system user interface provides the capability to monitor and command the Metasys system using graphics. To navigate through the system, see Navigating Graphics in View Mode.

To monitor your Metasys system using graphics:

Procedure

  1. Display graphics to show the status/state of your system components.
  2. Navigate through the system.
  3. To command objects/items using graphics, right-click on the symbol in View mode and select the desired command.

Results

Note: Right-clicking has no effect on Button Symbols.