Copying an Existing Graphic - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

About this task

Note: This is available when using the SCT only.

Procedure

  1. Click an existing graphic item in the Navigation Tree.
  2. On the Edit menu, select Copy.
  3. Click in the navigation tree where the new graphic is to appear.
  4. On the Edit menu, select Paste and name the new graphic.