About this task
To bind Switch symbols to objects:
Procedure
- Double-click the Switch symbol. The Binding Information dialog box appears.
-
Use the information in the following table to edit the fields.
Table 1. Dynamic Switch Options Field
Description
Object
Allows you to type in the Item Reference of the object you want to bind to the Switch. Or, lets you click the Browse icon to launch a tree browser to select the object to bind to the Switch.
Attribute
Allows you to select the object’s attribute to bind to the switch.
Number of States
Allows you to choose the number of states (2 or 3) the switch has.
State 0/1/2
Allows you to choose the text associated with each state.
OK
Accepts changes.
Cancel
Cancels changes.