Dynamics: Fans - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

About this task

To bind Fan symbols to objects:

Procedure

  1. Double-click the Fans symbol. The Binding Information dialog box appears.
  2. Use the information in the following table to edit the fields.
    Table 1. Fan Dynamics Options

    Field

    Description

    Object

    Allows you to type in the Item Reference of the object you want to bind to the Fan. Or, lets you click the Browse icon to launch a tree browser to select the object to bind to the Fan.

    Attribute

    Allows you to select the object’s attribute to bind to the fan.

    Clockwise/Counter-Clockwise

    Selects if the Fan symbol spins in a clockwise or counter-clockwise direction.

    OK

    Accepts changes.

    Cancel

    Cancels changes.