Adding Text Blocks - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

About this task

To add text blocks in Edit mode:

Procedure

  1. Click the Text icon on the UGT Toolbar.
  2. Click the workspace to select a location for the text. The text block appears.
  3. Click the Select icon from the toolbar and double-click on the text block. The edit text box appears.
  4. Type in the text box and click OK.
  5. Select the Select icon on the UGT Toolbar.
  6. Select the text block and drag the sides to resize the block.