Dynamics - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Dynamic symbols display the status of bound objects. If you select a single item or multiple items in the navigation tree and drag a dynamic symbol to the workspace, the UGT creates one symbol per item and binds each symbol to an item.

The dynamics category includes the symbols listed in the table below.

Table 1. Dynamics

Dynamics Type

Symbol

Animation

Fans

Fan/pump blades spin or remain stationary.

Basic Shapes (Square, Circle, and Triangle)

Colors change.

Switch (2 or 3 State)

Switch changes positions.