Drag and Drop Shortcuts - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Consider the following shortcuts when dragging and dropping items to the Graphic Workspace:

  • If you select a Graphic Object in the navigation tree and then drag a button to the graphics workspace, the UGT creates a button already bound to the selected Graphic object.

  • If you select multiple field points in the Navigation Tree and drag a Value Display Box to the graphics workspace, the UGT creates multiple Value Display Boxes each bound to a field point.

  • If you select multiple field points in the navigation tree and drag a dynamic symbol or gauge to the graphics workspace, the UGT creates multiple symbols each bound to a field point.

  • If you select multiple field controllers along with a Graphic object in the navigation tree and drag a button to the graphics workspace, the UGT creates buttons for all the controllers. All buttons have the appropriate Alias string already entered.

  • To change the binding information for a symbol or to add binding information (if you drag and drop a symbol without selecting anything in the navigation tree), see Binding Symbols to Objects in Edit Mode.