Opening the Trend Module from a Graphic - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

About this task

Note: You can open the Trend Module from a User Actions Panel or from the Graphics+ Display Control tool.

Procedure

  1. Open a Graphics+ object.
  2. To open the Trend Module from a User Actions Panel, right-click a graphic element to open its User Actions Panel. Supported elements include value boxes, room status elements, the LCD display within a Room Control Module, basic shapes, and gauges.
  3. Click View Trend. If more than one trend is available, click View Trend, then select from the list of trended attributes that appear in the submenu. The Trend Module loads and plots the trend data.
    Note: If View Trend does not appear in the User Actions Panel, this object has no trend extension.
  4. For more details, see Trend Module.
  5. To open the Trend Module from the Graphics+ Display Control tool, click the Tools drop-down arrow. The Trend option appears.
  6. Click Trend. The Trend Module appears either blank (no trend data selected) or replots the trend data for the objects you selected earlier.