Monitoring and Commanding Items Using Graphics - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

About this task

Note: The Site Management Portal UI provides the capability to monitor and command the Metasys system from a graphic.

To monitor your Metasys system using graphics:

Procedure

  1. Open a graphic to display the current status/state of system components.
  2. Navigate through the system.
  3. To command Metasys objects or items using graphics, right-click the graphicelement to open the User Actions Panel and click More Commands. Select fromthe available commands. To change the value of a Metasys object or item from aninline command box, click inside the box, type a new value, and press Enter. Forinformation on the runtime behavior of a particular graphic element, refer to theGraphics+ Runtime Help (LIT-12011708).