Zoom Operations - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

You can zoom in the chart by holding down the mouse and sliding across the chart (either to the left or to the right). This action activates drag zoom. Zoom works for values on the x-axis, not values on the y-axis. To zoom out, click the Zoom Out link that appears in the upper right corner on a zoomed chart.

You can also zoom from the horizontal scroll bar by clicking and dragging on the ends of the scroll bar.