User Actions Panel - Metasys - LIT-12011942 - Software Application - ODS Server - 10.1

Metasys Open Data Server Help

Brand
Metasys
Product name
ODS Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Language
English

You can open the User Actions Panel for a graphic element by right-clicking the graphic element. The User Actions Panel is a submenu of options that appears adjacent to the graphic element (Figure 1). The panel in the Site Management Portal UI supports three actions: View, Command, and Trend (SCT only supports View; Trend only appears for trended objects). To view the Focus window for the object, select its name (for example, ZN-SP). To command the object, select More Commands. To view trend data for the object in the Trend Module, select View Trend. If more than one attribute is trended, select View Trend, then click the attribute name. User access to all three actions is set with security levels in the Security Administrator System.

Figure 1. Opening a User Actions Panel