Behaviors - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Many elements of Graphics+ graphics support built-in or configurable behaviors.

Elements that support behaviors can flash if the bound object is in an alarm or warning state, change color based on the bound object's state or status, or show or hide depending on the bound object's state or status.

In the Metasys UI, the elements of the Graphics+ graphic display the behaviors as the bound object's state or status changes.

Note: Support of behaviors is limited in SCT.