Schedule Commands - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Table 1. Schedule Commands

Command Name

Number of Parameters

Description

Disable

None

The Disable command stops all future scheduled events. Neither the Weekly Schedule nor the Exception Schedule run again until the Schedule object is re-enabled. While disabled, the status log in the Scheduled Items view lists the object as disabled. The schedule remains disabled until re-enabled.

Enable

None

The Enable command allows the Schedule object to resume normal scheduling operation. The Schedule object starts the schedule as soon as it is enabled. When it is re-enabled, the Schedule object writes its current value to the scheduled items.