Notification Class Commands - Metasys - LIT-12011942 - Software Application - ODS Server - 10.1

Metasys Open Data Server Help

Brand
Metasys
Product name
ODS Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Language
English

The table below lists the commands supported by the Notification Class Object.

Table 1. Notification Class Object Commands

Command Name

Parameters

BACnet Supported

Add Recipient

See Recipient List.

Yes

Disable

0

No

Enable

0

No

Remove Recipient

See Recipient List.

Yes

Only supported by the BACnet Notification Class.