Notification Class Attributes - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

This object contains attributes common to many Metasys system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab, the Diagnostics tab (if applicable), and any other tab specific only to this object. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).

Click the attribute name in the table for a description of the attribute.
Note: In the notes and BACnet notes columns, attributes marked with the letter C are configurable, and attributes marked with the letter W are writable.
Table 1. Notification Class Object Attributes - Focus/Configuration Tab

Attribute Name

Notes

BACnet Notes

Initial Value

Values/Options/Range

Description

Ack Required

C,W

W

False,

False,

False

To Offnormal

To Fault

To Normal

Uses BAC Event Bits (Set 525).

Notification Class Object

     

0 to 4,294,967,295

Priority

C,W

W

120

200

70

To Offnormal

To Normal

To Fault

Range = 0 to 255

Route to Metasys

C,W

Not supported

True

True, False

Send Notifications to Supervisor

C,W

Not supported

True

True, False

Determines whether or not the Notification Class object routes alarms to the supervisory device.

Table 2. Notification Class Object Attributes - Recipient List Tab

Attribute Name

Data Type

Notes

BACnet Notes

Initial Value

Values/Options/Range

Recipient List

List of value sets

C,W

W

 

See Recipient List.

Uses BAC Day Bitset (Set 176), Recipient Choice (Set 526), and BAC Event Bits (Set 525).