Multistate Input Commands - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The table below lists the commands supported by the Multistate Input Object.

Table 1. Multistate Input Object Commands

Command Name

Parameters

Description

Disable Alarms

None

Enable Alarms

None

In Service

None

Note: For BACnet objects, support of this command is dependent on the ability to write the Out Of Service attribute.

Out of Service (Command)

The value to be written to the Present Value attribute.

For BACnet objects, support of this command is dependent on the ability to write the Out Of Service attribute.

Temporary Out of Service

The value to be written to the Present Value attribute, along with the hours and minutes that the out of service state is temporarily active.