Loop Commands - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The table below lists the commands supported by the Loop Object.

Table 1. Loop Commands

Command Name

Parameters

Description

Disable Alarms

None

Disables all types of alarming: alarm extensions, BACnet intrinsic alarming, and BACnet Event Enrollment objects. This command restores the previous Event Enable values.

Enable Alarms

None

Enables all types of alarming: alarm extensions, BACnet intrinsic alarming, and BACnet Event Enrollment objects. This command sets the Event Enable values to False, False, False.

In Service

None

Places the PID loop object algorithm in service.

Manual Tuning

None

Enables or disables the ability to change gain values of the PID Loop object, including Proportional Constant, Derivative Constant, Integral Constant, Bias, Maximum Output, and Minimum Output.

Out of Service

Real value

Places the PID loop object algorithm out of service. The value specified in the command is written to the JCI Out of Service Value Reference. The Present Value of the Loop object assumes the value of the JCI Out of Service Value Reference while out of service.