Lighting Output Attributes - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

This object contains attributes common to many Metasys system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab for this object. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).

Note: In the Notes column, letters for the attributes indicate the following: C - Configurable, N - Value Not Required, W - Writable.
Table 1. Lighting Output Attributes

Attribute Name

Notes

Initial Value

Values/Options/Range

Description

Blink Warn Enable

C, W

  True (enabled) or False (disabled)

Indicates whether the blink warning system is enabled. The blink occurs when a Warn, Warn Reliquish, or Warn Off command is issued to the Lighting Output object. Set to False to turn off the blink feature.

COV Increment

C, W

   

Specifies the minimum change in Present Value that causes a COV Notification to be issued to subscriber COV clients.

Default Fade Time

C, W

0

 

Indicates the default fade time value from the BACnet lighting output object, if present. The value is expressed in milliseconds.

Default Ramp Rate

C, W

0.0

 

Indicates the object's default ramp rate, if present. The rate is expressed in percent-per-second. The range of allowable ramp-rate values is 0.1 % to 100.0 % per second.

Default Step Increment

C, W

0.0

 

Indicates the amount to be added to the Tracking Value when the Lighting Command property is written with a step request.

Display Precision

C, W

100ths

 

Indicates the number of decimal places to display for the Present Value.

Egress Active

    True (active) or False (inactive)

Indicates whether the egress time is active. The egress time is in effect when a Warn, Warn Reliquish, or Warn Off command is issued to the Lighting Output object. Set to False to inactivate the egress time.

Egress Time

C, W

0

 

Specifies the value of the object’s egress time property, if present. The egress time is expressed in seconds.

Feedback Value

 

0.0

 

Indicates the actual value of the BACnet lighting output within the normalized range.

In Progress

     

Indicates the current state of the lighting output. Possible states include Idle, Fade-Active, Ramp-Active, Not-Controlled, or Other.

Instantaneous Power

     

Indicates the power consumption of the load that the Lighting Output object is controlling at this very moment. Units are in kW.

Lighting Command

C, W

   

Indicates the currently active lighting command. Possible states include Idle, Fade-Active, Ramp-Active, Not-Controlled, or Other. This attribute appears only in the Snapshot Focus view.

Lighting Command Default Priority

C, W

   

Indicates the default command priority used for sending lighting commands.

Lighting Command Display

     

Lists the fields used for commanding the Lighting Output object.

Max Actual Value

C, W

   

Specifies the physical output level that corresponds to a Present Value of 100.0%. This value is always a positive number in the range of 1.0% to 100.0%.

Min Actual Value

C, W

   

Specifies the physical output level that corresponds to a Present Value of 1.0%. This value is always a positive number in the range of 1.0% to 100.0%.

Object Identifier

     

Specifies the unique numeric code used by the BACnet device to identify the object.

Out Of Service

C, W

   

Indicates whether the Lighting Output object is currently Out of Service. When Out of Service is True, you can change the present value and reliability of the Lighting Output object.

Power

     

Indicates the power consumption of the load that the Lighting Output object is controlling. Units are in kW.

Priority Array

     

Lists values of the object in level of importance.

Profile Name

 

0-Object-LightingOutput

 

Specifies the name of the BACnet profile to which the Channel object uses.

Reliability

C, W

Reliable

Uses Reliability (Set 503).

Represents the reliability of the Present Value. If the Input Reference becomes unreliable, the trend extension monitoring the input becomes unreliable.

Remote Reliability

   

Represents the reliability of the remote object's Present Value.

Status Flags

     

Indicates the general status of the object in BACnet terms and contains four independent states.

The four flags are:

In Alarm—False if the Event State attribute value is Normal; otherwise, the In Alarm flag is True. (Set only by BACnet Intrinsic Alarming.)

Fault—True (1) if the Reliability attribute is not reliable; otherwise, the Fault flag is False.

Overridden—Overridden flag is True if the Present Value is overridden from the hardware source level.

Out of Service—Out of Service flag is True if the Out of Service attribute value is True; otherwise, the Out of Service flag is False.

Tracking Value

C, W

0.0

 

Indicates the controlled value of the physical lighting output in percent.

Transition

C, W

 

None, Fade, Ramp

Stores the value read from the BACnet lighting output object’s transition property, if present.