Lighting Output Object - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Menu Selection: Insert > Object > Lighting Output

The Lighting Output object allows a third-party BACnet workstation to represent a Lighting Output object in a BACnet field controller. The Lighting Output object represents in a linearized percentage the externally visible characteristics of a lighting output level. By adjusting the present value of this object, you can change the brightness level of banks of controlled lights. Typically, the adjustment value is from 5% to 85%.

User commands to the Lighting Output object provide special lighting-specific functions such as ramping, stepping, and fading. The lighting command also provides a blink-warn mechanism to notify room occupants that the lights are about to turn off. The blink-warning mechanism is internal to the Lighting Output object type and may cause a controlled set of lighting banks to blink on and off or issue a notification.