Life Safety Zone Commands - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The table below lists the commands supported by the Life Safety Zone Object.

Table 1. Binary Input Commands

Command Name

Number of Parameters

Description

In Service

 
Note: For BACnet objects, support of this command is dependent on the ability to write the Out Of Service attribute.

Out of Service

The value to be written to the Operation Expected.

Note: For BACnet objects, support of this command is dependent on the ability to write the Out Of Service attribute.