Life Safety Point Object - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The Life Safety Point object’s attributes represent the state of smoke detectors, fire detectors, security alarms, and similar devices. As a Life Safety Point, the state of this object can be one of 24 states.

The Life Safety Point object is a standardized object that represents a BACnet Safety Point Object as defined in the 2008 BACnet specification.