The table below lists the commands supported by the Channel Object.
|
Command Name |
Parameters |
Description |
|---|---|---|
|
Adjust as Bit String |
Value |
Writes the current value of the Present Value attribute to the third-party BACnet Channel object. Specify either bit string value: 0 or 1. |
|
Adjust as Boolean |
Value |
Writes the current value of the Present Value attribute to the third-party BACnet Channel object. Specify either boolean value: True or False. |
|
Adjust as Character String |
Value |
Writes the current value of the Present Value attribute to the third-party BACnet Channel object. Specify a character string value with a maximum of 64 characters. |
|
Adjust as Date |
Date or No Date |
Writes the current value of the Present Value attribute to the third-party BACnet Channel object. Specify a future date or select No Date for an unspecified date. The other date parameters presented on the dialog box are not available. |
|
Adjust as Double |
Value |
Writes the current value of the Present Value attribute to the third-party BACnet Channel object. Specify a double data type in the range of -1.79769E308 to 1.79769E308. |
|
Adjust as Enumeration |
Value |
Writes the current value of the Present Value attribute to the third-party BACnet Channel object. Select from the drop-down list of possible enumeration states in the range of State 0 to State 31. For values over State 31, use the Adjust as Unsigned Integer command instead. |
|
Adjust as Object ID |
Type, Value |
Writes the current value of the Present Value attribute to the third-party BACnet Channel object. Select the type of BACnet object from the drop-down list. Specify a BACnet Object ID in the range of 0 to 4194303. |
|
Adjust as Octet String |
Value |
Writes the current value of the Present Value attribute to the third-party BACnet Channel object. Specify an octet string data value with or without dashes including leading and trailing zeroes, such as 00-11-22-33-44-55-66-00. |
|
Adjust as Real |
Value |
Writes the current value of the Present Value attribute to the third-party BACnet Channel object. Specify a real number value in the range of -3.40282E38 to 3.40282E38. |
|
Adjust as Signed Integer |
Value |
Writes the current value of the Present Value attribute to the third-party BACnet Channel object. Specify a signed integer data value in the range of -2.14748E9 to 2.14748E9. |
|
Adjust as Time |
Hour, Minute, Second or No Time |
Writes the current value of the Present Value attribute to the third-party BACnet Channel object. Use the time control to specify an hour, minute, and second value in the format HH:MM:SS, or select the No Time check box for an unspecified time. |
|
Adjust as Unsigned Integer |
Value |
Writes the current value of the Present Value attribute to the third-party BACnet Channel object. Specify an unsigned integer data value in the range of 0 to 4.29497E9. |
|
Disable Alarms |
None |
Disables all types of alarming: alarm extensions, BACnet intrinsic alarming, and BACnet Event Enrollment objects. This command restores the previous Event Enable values. |
|
Enable Alarms |
None |
Enables all types of alarming: alarm extensions, BACnet intrinsic alarming, and BACnet Event Enrollment objects. This command sets the Event Enable values to False, False, False. |
|
Release |
None |
Releases the identified command priority from the specified, writable attribute, and allows it to be controlled by the next highest priority. |