Scheduling the Enabled Audit Level - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

About this task

To schedule the Enabled Audit Level based on time using the Scheduling feature:

Procedure

  1. Create a Schedule or display the desired Schedule.
  2. In the Scheduled Items tab, add the desired Engine or ODS and select the Enabled Audit Level attribute. Follow the steps in the Adding Scheduled Items procedure.
  3. On the Weekly Schedule tab, configure the events as desired. Follow the steps in the Adding Weekly Scheduled Events and Editing Scheduled Events procedures to schedule specific days and times to change the Enabled Audit Level. See the Engine Device Object or ODS Device Object ’s Enabled Audit Level attribute description for information on the levels you want to schedule.
  4. Click Save.