Scheduling a Trend Extension - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

About this task

Note: See the Trend Scheduling topic for information and examples on scheduling trend extensions.

Procedure

  1. Create a Schedule or display the desired Schedule.
  2. In the Scheduled Items list, add the desired object trend extension and the desired scheduled attribute. Follow the steps in the Adding Scheduled Items procedure. Make sure the trend extension is the key item. See Trend Extensions for information on the trend extension attributes you want to schedule.
  3. On the Weekly Schedule tab, configure the events as desired. Follow the steps in the Adding Weekly Scheduled Events and Editing Scheduled Events procedures to schedule specific days and times to perform the defined trending capability.
  4. Click Save.