Editing Exception Schedules - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Procedure

  1. Display a Schedule.
  2. From the Display Mode drop-down menu, select Exception Schedule.
  3. Click Edit.
  4. Double-click the exception schedule. The Exception Details dialog box appears.
  5. Make your modifications using the drop-down menus or for the calendar reference, click the Browse icon and select a calendar from the Select Items dialog box and click OK.
  6. Click OK on the Exception Details dialog box.
  7. Select the exception schedule in the exception list.
  8. Select and right-click the event in the time bar and select Modify Selected Event(s) from the menu. The Modify Event(s) dialog box appears.
    Note: Alternatively, you can double-click an event to open the Modify Event(s) dialog box.
  9. Select the starting time (hour and minute), and a value for the event using the check boxes and drop-down menus and click OK.
  10. Repeat Step 4 through Step 9 as necessary.
    Note: To change the value of an event, select and right-click an event and select a value from the menu.
  11. Adjust the start and end times of events by dragging the edge of the event to the right or left.
  12. Click Save.
    Note: Once you click Save, the schedule object goes into effect and writes the new value to the scheduled object if necessary.