Creating a Schedule or Calendar - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

About this task

Note:
  • The procedure for creating a schedule or a calendar in offline mode (using SCT) is the same as the online procedure using the Object. See Metasys Modes for more information about the modes of operation.
  • You cannot create schedules or calendars in an FAC from SCT or SMP.

Procedure

  1. From the Insert menu, select Object. The Insert Object Wizards appears.
  2. Select Schedule or Calendar and follow the Insert Object Wizard instructions.
    Note: Add extensions to the schedule or calendar at the wizard prompt, if desired. See Extensions.