Adding Scheduled Items - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Procedure

  1. Display a Schedule.
  2. From the Display Mode drop-down menu, select Scheduled Items.
  3. Click Edit.
  4. Click the add (green plus) button.
  5. Select one or more items from the Select Item dialog box and click OK.
    Note: To select multiple items, use the Control or Shift key.
  6. The system automatically chooses the default attribute for each item you selected. To choose a different attribute, click the Browse icon and select the attribute that you want to schedule.
  7. Click Save.
    Note: The first item in the list of scheduled items (Table of Scheduled Items) determines the data type used when the schedule writes values to the attributes of the scheduled item.