The scheduling feature has a weekly schedule that provides a schedule for each day of the week, Monday through Sunday. Each daily schedule begins at 00:00 and ends at 23:59. Each day consists of events that initiate the writing of values to the referenced attributes of the scheduled items based on the day of the week. For example, you can schedule a fan to start at 7:00 and stop at 22:00 on Mondays.
To edit the weekly schedule, double-click or right-click the weekly schedule. Right-clicking brings up the context menu (see Table 2).