Schedule - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The Schedule Object resides in an Engine or FAC and is the internal basis for the Scheduling feature. Create a Schedule and use the Scheduling feature to define the items and times when the Schedule writes values to the referenced attributes of the Scheduled Items. Each schedule includes the following:

  • a view of today’s schedule that shows what actions the schedule is currently configured to perform today, including the Default Schedule Command. This view is not available in the SCT.

  • a weekly schedule that uses events for each day (Monday through Sunday) to configure the times when the Schedule writes values to its referenced attributes (Scheduled Items)

  • an exception schedule that uses events to configure exceptions to the weekly schedule (optional)

  • a list of items that the schedule controls (referenced by the schedule, called Scheduled Items) (optional)

  • an effective period that optionally allows you to activate or inactivate the schedule for a selected period of time

Use the scheduling feature to:

The following tables describe the functions of the Schedule View’s buttons and attributes and right-click menu.

Table 1. Schedule Button Functions

Button

Function

Edit

Opens Edit mode

Effective Period

Click the Browse icon to open the Effective Period dialog box which allows you to specify the From and To values for the effective period.

Schedule Output Type

Binary, Analog, Multistate, Derived from Values — each of these choices brings up unique choices in the Default Schedule Command and State Text fields.

Default Schedule Command

Binary: Release option or a choice of Off and On

Analog: Release option or a choice to input a number

Multistate: Release option or a choice of State 0 to State 31

Derived from Values: Release option or a choice of Off and On

Note: If the Default Schedule Command is set to Release, the scheduling feature’s control over the scheduled items ends. Release should only be used for the Default Schedule Command if the scheduled items support the Release command.

States Text

Allows you to specify the state of the selected event, which is unique for each Schedule Output Type.

Display Mode

Allows you to toggle between views: Today's Schedule, Weekly Schedule, Exception Schedule, or Scheduled Items.

Table 2. Schedule Right-click Menu (this menu is accessible only when Edit mode is used)

Menu Option

Description

Display Mode - Weekly Schedule

Binary

The States Text selection controls the right-click menu. For example, select between Off and On, Off and Reset, Absent and Present, Active and Inactive, or Alarm and Normal.

Add Event(s)

Opens the Define New Event(s) dialog box and allows you to add an event to the schedule.

End Event

Allows you to specify an event end time. The end time corresponds to the location of your mouse cursor when you opened the menu. Drag the end of the event to adjust the end time.

Analog

Right-click and select Add Event(s), or select an event, right-click, and select Modify Selected Event(s). Add Event(s) allows you to specify the Day or Days, Hours, Minutes and Value of a new event. Modify Selected Event(s) allows you to modify the Hours, Minutes, and Value of an existing event.

Add Event(s)

Opens the Define New Event(s) dialog box and allows you to add an event to the schedule.

End Event

Allows you to specify an event end time. The end time corresponds to the location of your mouse cursor when you opened the menu. Drag the end of the event to adjust the end time.

Multistate

The States Text selection controls the right-click menu. For example, toggle between Not Operating, Normal Start, Heating, Cooling, Fan Only, or Minimum DAT Control.

Modify Selected Event(s)

Opens the Modify Event(s) dialog box and allows you change the times and value of the selected event. You can also double-click an event to access the Modify Event(s) dialog box.

Delete Selected Event(s)

Deletes the selected event.

Display Mode - Scheduled Items

All Scheduled Output Types

Choose between Make Key Item or Remove Item.