Effective Period - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The effective period defines the active or inactive date range for a schedule (weekly and exception schedule) using the date range rules. In Edit mode, the Browse icon opens the Effective Period dialog box. By default, a schedule is always active.

For example, you can create two schedules with the same items/objects and configure one for the heating season and the other for the cooling season. Then you can define the effective period of the heating schedule from October through March and the cooling schedule from April through September of each year.