Binary Value Object - Metasys - LIT-12011942 - Software Application - ODS Server - 10.1

Metasys Open Data Server Help

Brand
Metasys
Product name
ODS Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Language
English

Menu Selection: Insert > Object > BV

BV objects have similar software characteristics and capabilities to a Binary Input Object; however, Binary Value objects are not associated with any physical hardware and are the result of a control process or operator entry. This object allows you to hold a binary value for other objects to reference. For example, an Interlock can reference and base its operation on a binary value such as duty/standby.

For general information on Metasys system objects, see Common Object Attributes.