Analog Value Object - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Menu Selection: Insert > Object > AV

Analog Value (AV) objects have similar software characteristics and capabilities to Analog Input Objects; however, Analog Value objects are not associated with any physical hardware and are the result of a control process or operator entry. This object allows you to hold an analog value for other objects to reference. For example, an LON Integration Object can reference and base its operation on an analog value such as Outdoor Air Temperature Low Limit.

For general information on Metasys objects, see Common Object Attributes.