Analog Output Commands - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The table below lists the commands supported by the Analog Output Object.

For the Release Operator Override, Release, and Release All commands, if all Command Priorities have been released and a Relinquish Default is not defined, the supervisory controller gives control to the actual hardware. The Setpoint command is supported by N2 protocol only. Note that this command does not work on new controllers.

Table 1. Analog Output Commands

Command Name

Parameters

Description

Adjust

The value to be written to the Present Value. The value must be less than Max Present Value and greater than Min Present Value.

Important: Be aware that an operator Adjust command releases the actions of any processes running to the object in the NxE or FEC controllers that use Priorities 9 through 16. Consider this behavior when creating control strategies.

Disable Alarms

None

Enable Alarms

None

In Service

None

Note: For BACnet objects, support of this command is dependent on the ability to write the Out Of Service attribute.

Operator Override

The value to be written to the Present Value.

Out of Service

None

For BACnet objects, support of this command is dependent on the ability to write the Out Of Service attribute.

Release Operator Override

None

Release

Attribute name

Command priority

Release All

Attribute name

Important: The Release All command may not cause an immediate return to automatic operation. The Release All command clears all command priorities, including those that come from applications and features. When this happens, the output point goes to its Relinquish Default condition. In some cases, the application or feature may have sent a command that does not match Relinquish Default. In this instance, the output point does not end in the state that the applications or features intended. This situation can cause unexpected operation to occur; for example, a space could overcool or overheat, a fan might run longer than expected, and so on. If an operator has overridden an input, use the Release Operator Override command.

Setpoint

None

Writes the value to the permanent memory of the field device and may change the Present Value if there is no override.

Temporary Override

The value to be written to the Present Value attribute, in addition to the duration of the override in hours and minutes.

Overrides a point temporarily for a specified period of time. After the specified time period passes, the Override is automatically released.