Analog Output Object - Metasys - LIT-12011942 - Software Application - ODS Server - 10.1

Metasys Open Data Server Help

Brand
Metasys
Product name
ODS Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Language
English

The AO object’s attributes represent the external, visible characteristics of an analog output. This object integrates N1, N2, and BACnet controllers into supervisory controllers, resulting in:

  • a consistent interface to point objects for all controller types, so they appear as a homogenous set to the user interface

  • flexibility in point mapping

  • permanent update of setpoints in controllers. The user has the ability to write to the permanent memory of some controllers.

  • support for all Metasys controllers

  • For example, this object allows you to command a damper to a given position from a supervisory controller.

For general information on Metasys system objects, see Common Object Attributes.