LON Controller Commands - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The following table lists the commands supported by the LON Controller Object.

Table 1. LON Controller Commands

Command Name

Parameters

Description

Clear Statistics

None

Resets the statistics for the integrated LonWorks network. The contents of the Query Status message reflect these statistics:
  • Transmit Errors
  • Transaction Timeouts
  • Receive Transaction Full
  • Lost Message
  • Reset Cause
  • Node State
  • Version Number
  • Error Log
  • Neuron Model

Disable

None

Disables the entire LonWorks network integration. No requests are made to the field trunk and no data broadcasts to the network are processed.

Enable

None

Allows the integration to function normally.

Latch Statistics

None

Resets the statistics for the integrated LonWorks network. The contents of the Query Status message reflect these statistics:
  • Transmit Errors
  • Transaction Timeouts
  • Receive Transaction Full
  • Lost Message
  • Reset Cause
  • Node State
  • Version Number
  • Error Log
  • Neuron Model