This object contains attributes common to many Metasys system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab, the Diagnostics tab (if applicable), and any other tab specific only to this object. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).
|
Attribute Name |
Notes |
Initial Value |
Description |
|---|---|---|---|
|
Enabled |
C,W |
True |
If True, allows integration between the Metasys system and the LON controller. |
|
Graphic |
C,W |
Indicates the graphic associated with the object. | |
|
Graphic Alias |
C,W |
Indicates a portion of the graphic’s item reference, up to and including the name of the folder containing this object or the controller containing this point. |
|
|
Offline |
False |
Displays the offline or online status of connected hardware. The LonWorks network server updates this attribute value. |
|
|
Present Value |
Offline |
Displays the communication status of the object. | |
|
XIF Present |
Indicates whether a XIF file matching this controller’s Program ID was found. |
|
Attribute Name |
Notes |
Initial Value |
Description |
|---|---|---|---|
|
Command Count |
Displays the total number of commands sent to this controller. | ||
|
Error Log |
NOERROR |
Shows the error log according to the last standard LonWorks network Query Status message. | |
|
Lost Message |
0 |
Shows the number messages lost according to the last standard LonWorks network Query Status message. | |
|
Missed Messages |
Shows the number messages missed according to the last standard LonWorks network Query Status message. | ||
|
Neuron Model |
Neuron_3150 |
Shows the Neuron model according to the last standard LonWorks network Query Status message. | |
|
Node State |
Shows the state of the node according to the last standard LonWorks network Query Status message. | ||
|
Offline Poll Count |
0 |
Displays the total number of times this controller was sent a poll while offline. | |
|
Receive Transaction Full |
0 |
Shows the number of times the transaction full message appeared in the last standard LonWorks network Query Status message. |
|
|
Reset Cause |
Clear |
Shows the cause of the last reset according to the last standard LonWorks network Query Status message. | |
|
Reset Date |
Contains the date stamp of the last local Neuron statistics reset command. | ||
|
Reset Time |
Contains the time stamp of the last local Neuron statistics reset command. | ||
|
Total Messages to Device |
0 |
Displays the total number of messages sent to this controller. | |
|
Total Single Message Failures |
0 |
Displays the total number of failures for single messages sent to this controller. | |
|
Transaction Timeouts |
0 |
Shows the timeouts that appeared in the last standard LonWorks network Query Status message. | |
|
Transmit Errors |
0 |
Shows the number of transmit errors that appeared in the last standard LonWorks network Query Status message. | |
|
Version Number |
0 |
Shows the version number according to the last standard LonWorks network Query Status message. |