This object contains attributes common to many Metasys system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab and the Diagnostics tab. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).
|
Attribute Name |
Notes |
Initial Value |
Description |
|---|---|---|---|
|
Enabled |
C,W |
True |
If True, allows integration between the Metasys system and the IP field controller. |
|
Vendor Name |
W |
Identifies the manufacturer of the device. |
|
|
Model Name |
W |
Indicates the product code for the device. |
|
|
Fixed Boot Version |
Indicates the version of the Boot code in the field device. The Boot code is responsible for loading the Main code. |
||
|
Graphic |
C,W |
Object Name: Reference: |
Indicates the graphic associated with the object. |
|
Graphic Alias |
C,W |
Indicates a portion of the graphic’s item reference, up to and including the name of the folder containing this object or the controller containing this point. |