IP Field Controller Object - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The IP Field Controller object defines a standardized BACnet object with attributes that represent the external, visible characteristics of a device. Only one Device object exists in each IP Field Controller. The IP Field Controller object appears as a child of a BACnet Integration object.