BACnet Protocol Engine Commands - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The following table lists the commands supported by the BACnet Protocol Engine Object.

Table 1. BACnet Protocol Engine Commands

Command Name

Parameters

Description

Clear Statistics

None

Latch Statistics

None