The following table lists the commands supported by the BACnet Device Object.
| Command Name | Parameters | Description |
|---|---|---|
|
Rediscover Text Strings |
None |
Resets the States Text across a supervisory device by rediscovering text strings from all mapped BACnet objects. Note: When the Rediscover Text Strings command is sent from the Site Director device UI to another supervisory device and the UI is running on the supervisory device, you must close and restart the UI on the supervisory device in order for the text to appear correctly.
|
| Reset Field Device |
Type: Cold Start or Warmstart Password |
Resets the BACnet device. |
|
Sync Field Device Times |
None |
Sends a high-priority time synchronization command to child devices, based on the device mapper object's Manual Time Sync Type. |