BACnet Device Object - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The BACnet Device object defines a standardized BACnet object with attributes that represent the external, visible characteristics of a device. Only one device object exists in each BACnet Device.

Notes:
  • The Johnson Controls network engine device object includes attributes and methods not required by the BACnet Device object. For information on the network engine device object, see the Engine Device Object section.
  • The Object Type for this object is labeled Non-FEC BACnet Device in the software.