Printing the Entire Help System - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

About this task

The entire Help system is available for printing in Adobe PDF format.

To print the entire Help system:

Procedure

  1. If necessary, download Adobe Reader® (required to view the PDF file) from the Adobe Reader site.
  2. Go to the QuickLIT Product Information website.
  3. In the tree on the left, browse to Metasys System > Software .
  4. On the right side of the window, click Open Data Server Help (PDF format). The Help PDF opens in Adobe Reader.
  5. On the File menu of Adobe Reader, select Print.

Results

Note: This file is large (approximately 800 pages). Allow adequate time for downloading and printing.