Trend Sampling - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Trend sampling for the trend buffer occurs periodically (samples taken after a set time expires) if you set the Sample Interval to a value higher than zero. To sample based on COV reporting of the object, set the Sample Interval attribute to zero. You can stop or start sampling manually (using the Enable or Disable command) or control the start and stop with Interlocking a Trend Extension or scheduling. With interlocking, the trend samples are taken when a defined event occurs. If you use the scheduling feature, trend samples are taken at certain times on certain days.