Creating Extensions - Metasys - LIT-12011942 - Software Application - ODS Server - 10.1

Metasys Open Data Server Help

Brand
Metasys
Product name
ODS Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Language
English

About this task

Notes:

  • You cannot create an extension in online mode with Basic Access.
  • You can add only one load extension to an object.
To create extensions:

Procedure

  1. Select the item from the Navigation Tree and select Show Extensions from the Action menu.
    Note: Alternatively, you can create extensions when prompted upon completion of a wizard, or when the item is in the Panel Layout by selecting the tab for the extension and clicking new.
  2. Select New for the type of extension that you want to create. The corresponding Extension Wizard appears.
  3. Select the attribute that you want to associate with the item.
  4. Complete the information on the wizard screens. The screens vary depending on the type of extension you are creating.
  5. Select Finish on the summary page to create the extension.