Averaging Extensions - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The Averaging extension calculates the average, minimum, and maximum value of an attribute over a specific interval (for example, space temperature over 24 hours). The extension is able to sample Boolean, Integer, Unsigned, Enumerated, or Float attribute value types for any extendable objects within a BACnet device.

For more information on averaging extensions, see Averaging Attributes.