Multistate Alarm Extension - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The Multistate Alarm extension adds the alarming capability for an attribute with True or False, or Multistate data types, such as the Present Value of a Binary Input Object.

The Multistate Alarm extension detects the alarm with respect to a difference from a defined normal state and sets the Alarm State attribute of the object to which it is added. In addition, you can configure the Multistate Alarm extension to report alarms and True or False and/or Multistate events.