Alarm Extensions - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Alarm extensions monitor an attribute of an object and send alarms using the Alarm and Event Management feature. There are two types of alarm extensions, Analog Alarm and Multistate Alarm. Use the Analog Alarm extension to monitor attributes with real values. Use the Multistate Alarm extension to monitor attributes with True or False, or Multistate data types.

For general information on Metasys system objects, see the Object Help section.